Operator CameraRgbAreaBase

Operator Library: Hardware Platform

This operator represents the image data interface between a RGB area scan camera in RGB Camera Link base configuration mode and VisualApplets. This operator requires one VisualApplets resource of type CAM. Set the resource index for the camera in the resource dialog. The resource index 0 maps the camera to port A and the resource index 1 maps to the camera to port B. Check 'Allocation of Device Resources' for more information.

In the output link, the maximum possible image dimensions have to be specified. The size of the actual transfered images however may be less but must not exceed this parameterized maximum.

Available for Hardware Platforms
microEnable IV VD1-CL/-PoCL
microEnable IV VD4-CL/-PoCL

I/O Properties

Property Value
Operator Type M
Output Link O, image data output

Supported Link Format

Link Parameter Output Link O
Bit Width 24
Arithmetic unsigned
Parallelism 2
Kernel Columns 1
Kernel Rows 1
Img Protocol VALT_IMAGE2D
Color Format VAF_COLOR
Color Flavor FL_RGB
Max. Img Width any
Max. Img Height any

Parameters

UseDval
Type dynamic read/write parameter
Default Dval_Enabled
Range {Dval_Enabled, Dval_Disabled}

By setting this parameter to Dval_Disabled it is possible to support cameras which do not fully comply with the CameraLink specification. In disabled mode, control signals Lval and Fval are used to decode pixels. In enabled mode, the additional Dval signal is used. In general users should not modify this parameter!

Examples of Use

The use of operator CameraRgbAreaBase is shown in the following examples: